WaveGen Option Support
The oscilloscope application includes controls for the optional WaveGen built-in waveform generator available on those Keysight models that support this option. For those supported models, a separate license is required to enable the WaveGen functionality in the oscilloscope. Note that this license is an option for the oscilloscope instrument and it is required to use the WaveGen functionality with the oscilloscope application. For details on whether your oscilloscope supports this option, refer to the oscilloscope's user manual.
When a licensed WaveGen option is installed in the oscilloscope, the WaveGen option is shown on the Instrument Settings View panel (see below).